AXIS#.UNIT.POUT

Description

AXIS#.UNIT.POUT is used with AXIS#.UNIT.PIN to set application specific units in AXIS#.UNIT.POUT. This parameter is used as follows in the drive unit conversion:

  • For position, this parameter sets the units as Custom Units/revolution.
  • For velocity, this parameter sets the units as Custom Units/second.
  • For acceleration/deceleration, this parameter sets the units as Custom Units/second2.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

User units.

Range

1 to 4,294,967,295

Default Value

20
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
AXIS1.UNIT.POUT

5010h

02h

Unsigned32

-

-

Read/Write

No

AXIS2.UNIT.POUT

5110h

02h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.UNIT.POUT

6604

19CC

Unsigned32

Read/Write

-

AXIS2.UNIT.POUT

72140

119C

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.UNIT.POUT

6604

Unsigned32

Read/Write

-